Target devices
SH-4, SH-4A
*MMU (Memory Management Unit) is not supported.
Overview
University of Tokyo professor Ken Sakamura advocated the TRON project in 1984. The µITRON specification is one of the real-time operating system specifications standardized in the ITRON project established as a subproject of the TRON project. The µITRON specification is now a de facto standard in the Japanese embedded industry.
Renesas Electronics Corp. has been participating in the TRON project since the project was established. [HI series OS] is a realtime operating system for the Renesas H8/SuperH microcomputers which is compliant with uITRON specifications.
Refer to the T-Engine Forum website for detailed information on the ITRON specification and the µITRON specification.
T-Engine Forum Website
* T-Engine Forum holds the copyright on the μITRON Specification.
* TRON, ITRON, and μITRON do not refer to any specific product or products.
* The activities of TRON Association have been handed over to T-Engine Forum.
Taiwan Region (繁體中文)