Skip to main content

瑞薩電子針對汽車用途推出新一代微控制器RH850

為業界第一顆搭載嵌入式40nm快閃記憶體科技的MCU,具備低耗電量與高效能表現

TOKYO, Japan, February 29, 2012 — 先進半導體解決方案之頂尖供應商瑞薩電子(TSE:6723)宣佈推出針對汽車用途設計的全新RH850系列32位元微控制器(MCU)。RH850採用40奈米(nm)MONOS(金屬氧化氮氧化矽)嵌入式快閃記憶體,使瑞薩電子成為第一家於汽車市場中提供此一先進技術的半導體供應商。RH850系列MCU採用全新的RH850 32位元核心,以全球頂尖的32位元核心技術展現卓越的運算能力,提供超低功率處理科技所帶來的效益。

RH850是瑞薩科技與NEC電子於2010年4月合併後,由瑞薩電子延續兩家公司在汽車應用領域的傑出成就、產品可靠度與專業經驗所開發的一系列裝置中的最新產品。

瑞薩電子的RH850能滿足各汽車市場類別瞬息萬變的主流趨勢,其中包括從ASIL-A至ASIL-D等級的功能性安全需求、整合資訊安全功能與促進環保效益(如CO2減量)的低電耗功能等。RH850系列能夠以單核心提供64 MHz至最高320 MHz的效能等級,且多核心系統將可達到更高的整體效能。其嵌入式快閃記憶體提供256 KB至8 MB的選擇,更包含模擬EEPROM功能的資料快閃記憶區塊,並可提供12.5萬次「寫入/刪除循環」的耐久運作,資料至少可保留20年。

新產品系列將包含針對多種用途量身設計的產品陣容,並全面配備RH850的32位元核心架構。該系列也將擴展單核心、雙效能核心、雙核鎖步以及多核心架構,幾乎可滿足各種汽車市場對32位元MCU的所有效能與安全需求。瑞薩電子的系列概念結合可擴充的功能IP區塊、記憶體與針腳數,使客戶能在不需要變更應用程式軟體的情況下,彈性地擴充或縮減,進而選擇最符合其需求的產品。

為確保與客戶軟體的相容性,所有產品系列皆採用相同的平台開發概念,整個RH850產品系列皆重複使用相同的IP。

整合式開發環境(IDE)將支援RH850全系列產品,使客戶能從現今的產品更順利轉移至新平臺,並進一步減少整體的開發成本。

供貨

瑞薩RH850系列首批產品預定自2012年秋季起開始供應樣品,並預定自2014年起開始量產。(供貨情況如有變更,恕不另行通知。)

(Remarks)
All other registered trademarks or trademarks are the property of their respective owners.

關於瑞薩電子

瑞薩電子株式會社(TSE:6723)為全球第一的微控制器供應商,同時也是SoC系統晶片與各式類比及電源裝置等先進半導體解決方案的領導品牌之一。經由NEC電子(TSE:6723)與瑞薩科技的業務整合,瑞薩電子自2010年4月1日起正式營運,業務範圍則涵蓋了各種應用裝置的研發、設計與生產。總部位於日本的瑞薩電子,子公司遍及全球20個國家,如欲了解更多資訊,請造訪www.renesas.com


本新聞稿有關產品價格、規格及其他相關內容,為截至新聞稿發佈當時之資訊,日後如有變更將不另行通知。


End of content

Back To Top