A PFC (power factor correction) function corrects phase shifting between voltage and current by providing a triangular waveform current to inductor, then controlling the average current of the triangular waveform to be sinusoidal.
There are two modes as follows.
・Continuous current mode (CCM) --- for mid./large power over 600 W
・Critical current mode (CRM) --- for small/mid. power under 300 W
CCM PFC ICs and CRM PFC ICs are different from each other. Also, CRM mode can be single or interleaving.
|
![]() |

|
|
![]() |
Taiwan Region (繁體中文)